{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can I change the Nodename when cloning the controller application with SoMachine V4.3 / EcoStruxure Machine Expert via SD Card?
Issue
How can I change the Nodename of a Modicon M2xx PLC when cloning the controller application with SoMachine V4.3 / EcoStruxure Machine Expert via SD Card?

Product Line
SoMachine, EcoStruxure Machine Expert,
Modicon M241, M251, M262

Environment
Phsical PLCs

Resolution
This can be done by adding the following line in the script.cmd file in the SD Card before inserting it into the destination Modicon M2xx PLC.
The file is under \sys\cmd\script.cmd

The line to be added is:
SetNodeName "MyPLCNodeName"

Schneider Electric Global

Attachment(s)
scriptcmd.jpg [55.53 KB]
gateway_newnodename.jpg [118.67 KB]