Issue:
How to reset communication on a Serial modbus device when using the Modbus_IOScanner on a Serial_Line in a Modicon M238, M241, M251, M262 PLC?
Product Line:
Modicon M238, M241, M251, M262
Environment:
SoMachine V4.3, EcoStruxure Machine
Resolution:
One can use the ModbusSerialSlave Function block available under the SE_ModbusIOScanner library.
A rising edge to the xReset (BOOL) Input Pin will reset initiate a communication reset.
Depicted below is a representation of the Function Block in EcoStruxure Machine Expert v2.0.2.1:

How to reset communication on a Serial modbus device when using the Modbus_IOScanner on a Serial_Line in a Modicon M238, M241, M251, M262 PLC?
Product Line:
Modicon M238, M241, M251, M262
Environment:
SoMachine V4.3, EcoStruxure Machine
Resolution:
One can use the ModbusSerialSlave Function block available under the SE_ModbusIOScanner library.
A rising edge to the xReset (BOOL) Input Pin will reset initiate a communication reset.
Depicted below is a representation of the Function Block in EcoStruxure Machine Expert v2.0.2.1:
Released for:Schneider Electric Global