{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can we see how much CPU load is there on M241/M251/M262?
Issue
Is there a way to see how much CPU processor load there is on Modicon M241/M251/M262 by way of a function returning a value?
How do you program this in a POU in EcoStruxure Machine Expert / SoMachine?

Product Line
EcoStruxure Machine Expert, Modicon M241, M251, M262 PLCs

Environment
Programming Technique in EcoStruxure Machine Expert

Resolution
Yes, there is a way to return the CPU processor load using a Library called CmpSchedule.

In the Libraries->Add Library dialog, you will find it under Company->System under System->SysLibs:


The function in the library that returns processor load is SchedGetProcessorLoad:


An example of the program is as follows in Structured Text:

Declaration:
VAR
    pResult1       : RTS_IEC_RESULT;    //required pointer to the internal data location type (variable name is arbitrary)
    processorLoad  : UDINT;             //CPU load percentage
END_VAR


Code:
processorLoad := SchedGetProcessorLoad(pResult:=ADR(pResult1));


Note:
  • The value returned in "processorLoad" in his example is  is a percentage (in UDINT format).
  • It is recommended that processorLoad should remain lower than 70% (the lower the better). If this is not the case, then increase cycle times.

Schneider Electric Global