{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What types of external CTs can be used with Tesys T products?

Issue:
What types of external CTs can be used with Tesys T products?

Product Line:
NEMA and IEC Contactors and Starters

Environment:
Tesys T Motor Management

Resolution:
CTs for the TeSys T must meet precision class 5P and precision limit factor 15. As long as these CTs meet these requirements, any brand can be utilized.

Schneider Electric Global