To enable caps Lock press “Cap” icon. A green oval indicator above the “Cap” icon indicates that the Cap Lock function is enabled. To disable Caps Lock press “Cap” to change indicator to blue.
Press “Shift” icon to enable shift which will change the case of the next letter entered. A green oval indicator above the “shift” icon indicates that the shift function is enabled.
Press icon “123” to display number keyboard. Press “ABC” on number keyboard to return to letter keyboard.
How to login to ADMIN mode in the Accusine PCSP and PCSN HMI?
Recommended method to log in with default ADMIN password 3w7ADMN.
On alphabet screen have CAP key green, Shift blue.
Press 123 key
Press “3”
Press ABC
Press Shift, the oval will turn green
Press “W” (with caps lock on and shift on the character entered will be a lower-case w)
Press 123 key
Press “7”
Press “ABC” key
Press A, D, M, N press Enter.
This method works best when the number of capital letters is greater than the number of lower-case letters.
Released for:Schneider Electric Global