Electrical Designer
Job Description
Application Engineer- Order Engineering Team
This position is accountable for, but not limited to:
· Layout and configuration of switchgear.
· Design of control schemes, utilizing PLCs and/or relays, to accomplish automated transfer operations.
· Creation of electrical one line, elevation drawing, schematics and wiring diagrams using AutoCAD.
· Design of ground fault protective schemes, including those involving multiple sources.
· Generation of bills of material, and modification of standard assemblies as required to suit the application.
· Interpreting customer requirements by reading customer documents such as customer one line, specification, layout drawing etc
· Ensures assignments are within design, budget and schedule limitations.
· Communicates project concerns and suggestions, both verbally and in writing, with the Project Manager and Engineering Manager
· Participates as needed in proposal acceptance reviews, offering acceptance or recommendations for improvement on the systems engineering scope of work and labor hours estimated on the proposed project.
· Provide virtual technical support for shop floor for the orders engineered.
· Take up stretched assignments as and when needed.
· Should be able to work on Shift- Flexible timings support United states SE-shop floor
· Minimal travel may be required.
Required Competencies:
· Strong basic Electrical Engineering knowledge.
· Good verbal and written communication skills.
· Excellent interpersonal and customer relation skills.
· Excellent problem resolution skills.
· Ability to interpret basic front elevation, one-line, and schematic drawings.
· To work in a virtual environment. (without seeing the product physically, as Manufacturing Plants are in North America).
· Should be team player and be able to work in a multicultural team.
· Good interpersonal and customer relation skills.
Preferred Competencies:
· Knowledge of low voltage switchboard / switchgear design, installation, and Application
· Experience using AutoCAD.
· Familiarity with Relays & Its function.
· Knowledge on UL standards (UL1558 , UL891 ) is added advantage.
Behavioral Competencies:
· To be professional and ethical at all times. Exhibit a courteous, conscientious, and generally businesslike manner in the workplace.
· To be Passionate, Open and Respectful, Straightforward in one’s dealing and act with Integrity, to be Effective and deliver high performance and be pragmatic and fast.
Qualifications
Diploma with 1+ yrs OR BE/B.Tech in Electrical Engineering.
Schedule: Full-time
Req: 009ENA